Hi all
I want to connect an optical port with baud rate 300 to 1321x NCB board. But the board baud rate can only be set from 1200 to 38400 (as below). How can I change the baud rate to 300?
Thanks
/* SCI baud rate = BUSCLK/(16?Baud rate)
* Note that not all baud rates work for all clock rates. The actual baud rate
* may deviate too much from the RS232 specification.
*/
#ifndef gSystemClock_d
#define gSystemClock_d 16 /* 16 MHz. */
#endif
typedef uint16_t UartBaudRate_t;
#if gSystemClock_d == 8
#define gUARTBaudRate1200_c ((UartBaudRate_t) 0x01A1)
#define gUARTBaudRate2400_c ((UartBaudRate_t) 0x00D0)
#define gUARTBaudRate4800_c ((UartBaudRate_t) 0x0068)
#define gUARTBaudRate9600_c ((UartBaudRate_t) 0x0034)
#define gUARTBaudRate19200_c ((UartBaudRate_t) 0x001A)
#define gUARTBaudRate38400_c ((UartBaudRate_t) 0x0011)
#define gUARTBaudRate57600_c ((UartBaudRate_t) 0x0009)
#define gUARTBaudRate115200_c ((UartBaudRate_t) 0x0004) /* Might not work for all clients */
#endif
#if gSystemClock_d == 12
#define gUARTBaudRate1200_c ((UartBaudRate_t) 0x0271)
#define gUARTBaudRate2400_c ((UartBaudRate_t) 0x0139)
#define gUARTBaudRate4800_c ((UartBaudRate_t) 0x009C)
#define gUARTBaudRate9600_c ((UartBaudRate_t) 0x004E)
#define gUARTBaudRate19200_c ((UartBaudRate_t) 0x0027)
#define gUARTBaudRate38400_c ((UartBaudRate_t) 0x0014)
#define gUARTBaudRate57600_c ((UartBaudRate_t) 0x000D)
#define gUARTBaudRate115200_c ((UartBaudRate_t) 0x0007)
#endif
#if gSystemClock_d == 16
#define gUARTBaudRate1200_c ((UartBaudRate_t) 0x0341)
#define gUARTBaudRate2400_c ((UartBaudRate_t) 0x01A1)
#define gUARTBaudRate4800_c ((UartBaudRate_t) 0x00D0)
#define gUARTBaudRate9600_c ((UartBaudRate_t) 0x0068)
#define gUARTBaudRate19200_c ((UartBaudRate_t) 0x0034)
#define gUARTBaudRate38400_c ((UartBaudRate_t) 0x001A)
#define gUARTBaudRate57600_c ((UartBaudRate_t) 0x0011)
#define gUARTBaudRate115200_c ((UartBaudRate_t) 0x0009) /* Might not work for all clients */
#endif
#if gSystemClock_d == 16780
#define gUARTBaudRate1200_c ((UartBaudRate_t) 0x036A)
#define gUARTBaudRate2400_c ((UartBaudRate_t) 0x01B5)
#define gUARTBaudRate4800_c ((UartBaudRate_t) 0x00DA)
#define gUARTBaudRate9600_c ((UartBaudRate_t) 0x006D)
#define gUARTBaudRate19200_c ((UartBaudRate_t) 0x0037)
#define gUARTBaudRate38400_c ((UartBaudRate_t) 0x001B)
#define gUARTBaudRate57600_c ((UartBaudRate_t) 0x0012)
#define gUARTBaudRate115200_c ((UartBaudRate_t) 0x0009)
#endif
/*list of possible baudrates */
#define Baudrate_1200 gUARTBaudRate1200_c
#define Baudrate_2400 gUARTBaudRate2400_c
#define Baudrate_4800 gUARTBaudRate4800_c
#define Baudrate_9600 gUARTBaudRate9600_c
#define Baudrate_19200 gUARTBaudRate19200_c
#define Baudrate_38400 gUARTBaudRate38400_c
#define Baudrate_57600 gUARTBaudRate57600_c
#define Baudrate_115200 gUARTBaudRate115200_c
/* Default baud rate. */
#ifndef gUartDefaultBaud_c
#define gUartDefaultBaud_c Baudrate_38400
#endif
Hi bitasobhani,
Seems to me you can extend these tables yourself down to 300 baud. Probably the only reason this was not done is it is rare to use such low rates these days. Simply multiply the 1200 value by 4.
Thanks for reply
I added 300 baud rate to the table (as below). It works but receives bytes with error or some bytes are missed.
#ifndef gSystemClock_d
Hello,
If you are polling the SCI module for received data, you will need to periodically clear the COP timer whilst waiting. Otherwise it may be possible for COP timeout and reset to occur.
Additionally, during multiple byte send operations, you should also periodically clear the COP whilst waiting for the SCI buffer to become empty, ready to accept the next byte. The transmission time for each byte is 33 milliseconds.
Regards,
Mac
Thanks for reply
I am not polling the SCI module. I am using Interrupt routine for receiving bytes. But I receive wrong bytes with my added baud rate 300.
void BeeAppInit
(
void
)
{
...
Uart1_SetRxCallBack(Uart1RxCallBack);
Uart1_SetBaud(gUARTBaudRate300_c);
...
}
static void Uart1RxCallBack
(
void
)
{
Uart1_GetByteFromRxBuffer(&byte);
...
}