MC9S08LC60 VREFH and VREFL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08LC60 VREFH and VREFL

1,149 Views
rdazcal
Contributor III

Greetings all,

 

I'm using a MC9S08LC60 MCU and I have VREFH and VREFL pins available externally in the micro-controller.

 

I want to connect this pins to different values than VDD and VSS, but I read the following instruction in the data-sheet:

 

"When available on a separate pin, VREFL must be connected to the same voltage potential as VSSAD."

 

Why is that? Why would it be available externally and not be connected internally in the MCU if the user has no control over it?

 

And why VREFH can't be lower than 1.8V?

 

Thank you

Labels (1)
0 Kudos
Reply
2 Replies

751 Views
bigmac
Specialist III

Hello,

 

Having the VrefH and VrefL pins externally accessible would permit additional noise filtering to be applied - potentially very useful for 12-bit resolution mode.

 

The lower limit on VrefH is similar to the lower limit of Vdd.  I presume that, for an even lower VrefH level, the ADC accuracy would deteriorate to an unspecified level.

 

Regards,

Mac

 

0 Kudos
Reply

751 Views
rdazcal
Contributor III

I see....

 

Well, it makes sense....

 

Thank you bigmac

0 Kudos
Reply