很多年之前,利用贵公司的ISP1581开发了基于USB通讯的设备。现在,发现该设备在WIN10系统下无法使用,原因是ISP1581无WIN10的驱动。请问,公司里有开发适用于WIN10的该驱动程序么?或者,有之前改驱动的源代码么?
The ISP1581 is a very old device that is no longer supported.
Thanks
谢谢答复。
我知道ISP1581是很多年前的产品,目前已不提供技术支持了。那么,贵公司能提供之前该驱动的源代码么?我现在需要在WIN10下使用。如果可以的话,我自己再想办法重新编译生成。
谢谢!
Hi
Sorry all the information is now obsolete and no available