Hello,
I use HCS08 QE4 MCU along with OpenSource BDM. Suddenly I can't connect to MCU (I'm not aware that I did something wrong with my board where the MCU is at the time the problem appeared).
The program that is loaded in MCU is running correctly
I caught some waveforms. When I connect MCU to OpenSource BDM the waveforms are deformed:
http://gaminn.sweb.cz/MCU/bad.gif
http://gaminn.sweb.cz/MCU/bad2.gif
(voltage between GND and 3.3V appears on the line, edges of signal are not steep)
When I disconnect MCU the output signal of OpenSource seems not to be deformed.
Is there anything you can advise to me?
Thank you
Martin
Dear Gamin,
I'm not sure what the problem is but sometimes the BDM can have trouble connecting if the device is not programmed correctly.
You can try the technique here
You should also try unsecuring the device.
bye