Running KDS project for this part.
I find that the ADC analog pins voltage protect when input exceeds 1.6V approx.
VDD ,VDDA - 3.3V
VSS,VSSA - GND
Ran 8 and 16 bit configuration - Single ended 48Mhz clk ext
Jtag/uart/PDio all work as expected. Replaced IC same operation.
The lower 8 bits work in both configurations
until ADC input value reaches above 1.6V.
Is the 32QFN limited to half VDD input voltage for analog inputs and 8bit only?
Data sheet - VrefH and VrefL are connected to VDDA and VSSA respectively for this part.
Hi @CG-NXP
I hope you are doing well!
The MK20DX128 ADC should be capable of performing 16 bit conversions.
Could you help me with the following:
1 Code example with your ADC configuration.
2 Is the ADC configured to work with single-ended channels?
Best regards,
Diego.