I need a bootloader fo KL16 in produce product. the bootloader can use any UARTs of KL16 to download the firmware. IDE is IAR.
Whichone has a solution?
Thanks
Hello everyone:
I migrate the software from K16 to K17, so the KBOOT can be used, perfects. The hardware need to be uptated also.
thanks
Hi niu,
Thank you for your updated information, it's good.
If you still have question about this topic, please kindly let us know.
If your question is solved, please help to mark the correct answer, just to close this question.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi zhigang,
you may first download Kinetis Bottloader package from the below link:
http://www.nxp.com/products/reference-designs/kinetis-bootloader:KBOOT?&tab=Design_Tools_Tab
and then porting code to Kl26/KL16 base on example code in this package, say KL25.
also you can refer to guide in this package "Getting Started with the Kinetis
Flashloader" to learn how to porting it.
This question post may also helps you:
https://community.nxp.com/thread/450142
Wish it helps you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
THANK YOU VERY MUCH.
--
牛志刚
主页:Http://www.mnshanghai.com <http://www.mnshanghai.com/>
电话:021-35303166
手机:13817023673
You are welcome!
If your question is solved, please help us to mark the correct answer, just to close this question.
Thank you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Further more,
In the original version, the Bootloader is very powerfull, it's scanning all the possible link
I2C,SPI, CAN and UART
You need to modify the original version 2.0.0 to adapt it to you hardware.
check the files :
Hardware_init_Kxx.C files.
Peripherals_Kxx.C files
Peripheral_pinmux.h
regards
bertrand
thank you a lot. I'll try it.
--
牛志刚
主页:Http://www.mnshanghai.com <http://www.mnshanghai.com/>
电话:021-35303166
手机:13817023673
I just fished a bootloader for KV46 for a industrial system
Uart used at 256 Kb /sec.
adapted from 2.0.0 KInetis bootloader.
No modification needed for The Kinetis flashloader required.
Regards
Bertrand