gpio 1v8 pull up question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gpio 1v8 pull up question

621 Views
yan2anfei
Contributor III

hi ,

I have a imx6slevk, I set the SD3 clk as follow, the LVE bit is set ,but the voltage is 3.15v,Is anything wrong of my setup.

MX6SL_PAD_SD3_CLK__SD3_CLK 0x410059

and some gpio I had set the  LVE bit,and enable  internal pullup ,but  It's voltage is 3.3v isn't 1.8v.

I saw the i.Mx pins tool has a option of power group,but the option is gray and can't set. can the section  change to 1.8v.  

Labels (2)
0 Kudos
Reply
1 Reply

533 Views
Yuri
NXP Employee
NXP Employee

Hello,

 the following may be helpful:

LVE bit Pad control Register 

https://community.nxp.com/message/638173 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply