How can I modify the MAC address written on imx6 ROM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I modify the MAC address written on imx6 ROM?

953 Views
jackeyko
Contributor III

To change the MAC address, I had MAC Writh the following instruction as below:

[Mac Address Command for MFG Tool] --> MAC Address : 00:01:6F:01:FF:FF
<CMD state="Updater" type="push" body="$ ls /sys/fsl_otp ">Showing HW_OCOTP fuse bank</CMD>
<CMD state="Updater" type="push" body="$ echo 0x6F01FFFF > /sys/fsl_otp/HW_OCOTP_MAC0">write 0x6F01FFFF to HW_OCOTP_MAC0 fuse bank</CMD>
<CMD state="Updater" type="push" body="$ echo 0x0001 > /sys/fsl_otp/HW_OCOTP_MAC0">write 0x0001 to HW_OCOTP_MAC1 fuse bank</CMD>
<CMD state="Updater" type="push" body="$ cat /sys/fsl_otp/HW_OCOTP_MAC0">Read value from HW_OCOTP_MAC0 fuse bank</CMD>

I understand that it is can not be changed again if the address was used once,
Is there any way to translate them into instructions?

Labels (4)
0 Kudos
Reply
1 Reply

568 Views
Yuri
NXP Employee
NXP Employee

Hello,

 There are several options to configure the MAC : "the MAC address can be set through
the kernel command line, kernel device tree DTS file, OCOTP, or MAC registers set by
bootloader, such as U-Boot."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------