P&E GDB Server, Version 5.13.02.00
Copyright 2014, P&E Microcomputer Systems Inc, All rights reserved
Loading library C:\Freescale\KDS_2.0.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_1.1.7.201410171532\win32\gdi\unit_ngs_arm_internal.dll ... Done.
Command line arguments: -device=K60FX512 -startserver -singlesession -serverport=7224 -interface=USBMULTILINK -speed=5000 -port=USB1 -USE_CYCLONEPRO_RELAYS=0 -FORCE_MASS_ERASE=0
Device selected is k60fx512
User Specified Hardware Selection : Interface=USBMULTILINK and Port=USB1
Connecting to target.
P&E Interface detected - Flash Version 9.33
Can not enter background mode .
Unable to initialize PEDebug.
PE-ERROR: Failed to Initialize Target
Server running on 127.0.0.1:7224
Connection from "127.0.0.1" via 127.0.0.1
PE-ERROR: Target is not connected
Disconnected from "127.0.0.1" via 127.0.0.1
Target Disconnected.
Hello anju,
First if your board is a customer board , please be sure the JTAG interface design is right,
you can refer to the demo baord of k60 , for example the TWR-K60D100 board:
Then if the pcb is right , please take screenshot about how to configure the debug configuration on the KDS2.0 .
And there is a same question as yours , maybe it can hleps:JTAG connection problem
Hope it helps
Alice
Hello Alice,
I have attached the image of the jtag interface we are using.I have tried programming the K60 board pulling up the TDI pin also.But same programming error appears.The reset_b and EZP_CS pins are high. Earlier two or three times we programmed the processor without mass erasing it intially,so i hope the jtag interface is correct.But not now, the above said error appears.Please help.
Hello ,
You said some days before it can work well , and you if you have not change the board ,
it maybe the configuration have some problem when debug , please take a screenshot .
And please check the "Device Manager" of computer , check whether it detect it when you connect the board.
And you can also connect the PIN2 to power to have a try .
Alice