Hi,
I have a FRDM-K22F demo board, also use SDK to develop FW. I checked all UART example, seems that all UART example run in query mode. Do you have the UART interrupt example?
In the further, I also use MK22F1M0 chipset to develop CAN bus function, do you have CAN interrupt example?
Best regards,
Kent
Iva,
I checked the uart_non-blocking_example in the "C:\Freescale\KSDK_1.3.0\examples\frdmk22f\driver_examples\uart\uart_non_blocking", but seems that it still is loop-query mode? Don't see any "Interrupt flag", "IRQHandler" ,etc source code?
Best regards,
Kent
Hi Kent,
thank you for your question.
We have UART example with non-blocking method, which is located under C:\Freescale\KSDK_1.3.0\examples\frdmk22f\driver_examples\uart\uart_non_blocking
and about CAN interrupt example I think this could help you void FLEXCAN_DRV_IRQHandler (uint8_t instance)
In case of any issue please let me know.
Thank you,
Have a nice day!
Iva