Hi all, I just downloaded Yocto/Oe Poky 1.7 3.14.28-1.0.0_ga (following the instruction published on Freescale's i.mx6 website).
Googling around I found that in order ti use uClibc instead of eglibc or glibc I've just to add "TCLIBC = "uclibc" to the local.conf file in the yocto build dir.
It seems that adding "TCLIBC = "uclibc" really forces 3.14.28 to be built using uClibc but unfortunately there are errors during the build process (isn't the case if I remove the TCLIBC option).
Does anyone built Poky 1.7 with uClibc ?
Does Freescale imx6qsabre poky supports uClibc at all ?
Do I've to do anything more than adding the TLIBC option in the local.conf file to enable uclibc usage ?
Thanks in advance for any help, Joel
Original Attachment has been moved to: Error.txt.zip
Hi Joel,
You could refer to the following thread, which explains some additional steps required to add uClibc support on Linux:
https://community.freescale.com/thread/342503
Such thread provides some links to free-electrons webpage; you could specifically refer to section “4.3. Customizing the uClibc configuration” of the link below:
http://free-electrons.com/~thomas/buildroot/manual/html/ch04.html#uclibc-custom
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------