Hi,
I am working with Codewarrior v10.6 and of MQX v4.0.
In my project I am working on ethernet as well as on SDCard.
Problem is both are not working simultaneously in Tower kit. Means whenever I am inserting SDCard into Tower K60D100M slot, ethernet port is not working in tower((LED on Socket is also not glowing)).When I am removing SDCard from Slot Ethernet Port is working (LED on Socket is also glowing).
I dont know why it is happening??
Is there any jumper setting that I need to do in TWRK60D100M for SDCard??Or is there any settings in userconfig.h file that I need to do??
Please note that both task are working fine individually but not working simultaneously.
I also have seen while using Ethernet SDcard cannot be used but cant get the solution and Link is not able to open.
Please help.:smileyconfused:
Hi,
Please check the below thread and let me know if this helps.
SD and Ethernet conflict (K60 Tower system)
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------