Hi,
I'm running a project succesfully in CW10.3, now I've updated to 10.5 and I get the following problem when trying to debug via ' download':
INF:CRC-16 Error in block. (File = $892C, Device = $2DD1)
It appears to compile and download without issue, however it falls over on checking?
We can debug using 'attach'.
What has changed here in CW10.5?? I would really like to use 'Download' debug method.
Cheers,
KMC
Hello Kevin:
Could you provide more details? What is the specific error you see?
If possible please share a screenshot of the issue. Also it is always good to try with a new bareboard project to determine if the problem is with CodeWarrior <-> debugger tool or specifc to your project.
Regards!
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Kevin,
can you mail me your project (Code) i can compile here , having CW 10.5 and PE USB Multilink Interface programming Hardware.
Thanks and Regards,
Robin
Hi Kevin,
May be this is useful for you ,please go through it.
CW10.5 debug problem > Cannot enter background mode. Check connections.
Thanks and Regards,
Robin