Hi,
I have CodeWarrior 7.3 installed on a Windows 7 machine and was able to get the USB TAP up and running by following AN4338.
I have now tried to install the standalone Flash Programmer 1.2 because I need some batch scripts to write different Srec files to different memory areas in my board (a 56F8366).
During the installation it complained about the drivers.
When I try to run it it erases the Flash and then gives a "CCCSClient::WriteMemoryDirect: Core not responding" message.
Loading through CodeWarrior works fine.
I have tried substituting the ccs folder with the ccs folder from my CodeWarrior installation and still nothing.
I have also tried the ccs folder from this post: Problem with CodeWarrior USB TAP and Win 7.
Still the same...
Thank you
Marianna S. Buschle
Solved! Go to Solution.
The CCS update in AN4338, only works for CodeWarrior 8.3, not for 56800E Flash Programmer. I will upload a new CCS update, please use this one to replace the CCS folder under both CW8.3 and Flash Programmer.
Works perfectly.
Thanks a lot
Best Regards
Marianna