What is the real memory address (like Row/Col/Bank/CS) with DDR contorller map

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the real memory address (like Row/Col/Bank/CS) with DDR contorller map

880 Views
shangregister
Contributor II

Hi sir,

Sorry sir My question is ,what is the Soc imx8m Address from for 0x4000_0000 to FFFF_FFFF (3GB)  represent with LPDDR4 Ram Address (like Row/Col/Bank/CS).

for example : Soc  imx8m Address 0x8000_0000 it located  start at (1GB)  ram software location but what is the (Row/Col/Bank/CS) at that moment is?

9.3.3.1.62 i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

Just said the Address setting.

and theMSCALE SERIES DDR Tool Release (V2.10)  too.

0 Kudos
Reply
1 Reply

824 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  The i.MX8M DDRC provides flexible address mapper logic to allow application specific mapping of row, column,
bank, and rank bits. 
 Use descriptions of Address Map Registers  (ADDRMAP0 - ADDRMAP11) of the i.MX8M DDRC

in the Reference Manual.

 

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply