Hi All,
We have a custom board built with T4 Series processor. I changed the NOR flash address from 0xE8000000 - 0xEFFFFFFF to 0xE0000000 - 0xEFFFFFFF and we connected 2 NOR Flash chip in Hardware side.
But, after changed the address of NOR flash memory address the Ethernet is not working in Linux but it's working in u-boot and NAND is working in Linux and not working in u-boot.
I needs to know, what are the things I want to carry when changed the NOR flash address. And also I provided my changes and please response If I anything I missed.
Currently used Document for NOR Flash,
https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
Table 110. NOR Flash Memory Map
Changed location,
Current,
#define CONFIG_SYS_NOR0_CSPR (CSPR_PHYS_ADDR(CONFIG_SYS_FLASH_BASE_PHYS \
+ 0x8000000) | \
CSPR_PORT_SIZE_16 | \
CSPR_MSEL_NOR | \
CSPR_V)
Modified,
#define CONFIG_SYS_NOR0_CSPR (CSPR_PHYS_ADDR(CONFIG_SYS_FLASH_BASE_PHYS \
+ 0x0000000) | \
CSPR_PORT_SIZE_32 | \
CSPR_MSEL_NOR | \
CSPR_V)
Current,
ranges = <0 0 0xf 0xe8000000 0x08000000 2 0 0xf 0xff800000 0x00010000 3 0 0xf 0xffdf0000 0x00008000>; nor@0,0 { #address-cells = <1>; #size-cells = <1>; compatible = "cfi-flash"; reg = <0x0 0x0 0x8000000>;
Modified,
ranges = <0 0 0xf 0xe0000000 0x00000000 2 0 0xf 0xff800000 0x00010000 3 0 0xf 0xffdf0000 0x00008000>; nor@0,0 { #address-cells = <1>; #size-cells = <1>; compatible = "cfi-flash"; reg = <0x0 0x0 0x0000000>;
Thanks & Regards,
VinothS.
Solved! Go to Solution.
Hello vinothkumar s,
Please modify dts as the following
ranges = <0 0 0xf 0xe0000000 0x10000000
For new IFC NOR Flash integration, you also need to modify IFC timing parameters configuration in include/configs/T4240RDB.h. #define CONFIG_SYS_NOR_AMASK IFC_AMASK(128*1024*1024) /* NOR Flash Timing Params */ #define CONFIG_SYS_NOR_CSOR CSOR_NAND_TRHZ_80
#define CONFIG_SYS_NOR_FTIM0 (FTIM0_NOR_TACSE(0x4) | \
FTIM0_NOR_TEADC(0x5) | \
FTIM0_NOR_TEAHC(0x5))
#define CONFIG_SYS_NOR_FTIM1 (FTIM1_NOR_TACO(0x35) | \
FTIM1_NOR_TRAD_NOR(0x1A) |\
FTIM1_NOR_TSEQRAD_NOR(0x13))
#define CONFIG_SYS_NOR_FTIM2 (FTIM2_NOR_TCS(0x4) | \
FTIM2_NOR_TCH(0x4) | \
FTIM2_NOR_TWPH(0x0E) | \
FTIM2_NOR_TWP(0x1c))
#define CONFIG_SYS_NOR_FTIM3 0x0
Please refer to https://community.nxp.com/docs/DOC-333350 for details.
Thanks,
Yiping
This is the problem with memory map in flashing (changed 16 bit to 32 bit ) and gives unwanted behavior (Ethernet working in u-boot but not in linux as well as NAND working in Linux not in u-boot) . I configured address for FMAN as well as environment variable. There is no root cause, I closed this thread now. I start from working condition and do step by step to resolve this problem.
Regards,
VinothS.
Hello vinothkumar s,
Please modify dts as the following
ranges = <0 0 0xf 0xe0000000 0x10000000
For new IFC NOR Flash integration, you also need to modify IFC timing parameters configuration in include/configs/T4240RDB.h. #define CONFIG_SYS_NOR_AMASK IFC_AMASK(128*1024*1024) /* NOR Flash Timing Params */ #define CONFIG_SYS_NOR_CSOR CSOR_NAND_TRHZ_80
#define CONFIG_SYS_NOR_FTIM0 (FTIM0_NOR_TACSE(0x4) | \
FTIM0_NOR_TEADC(0x5) | \
FTIM0_NOR_TEAHC(0x5))
#define CONFIG_SYS_NOR_FTIM1 (FTIM1_NOR_TACO(0x35) | \
FTIM1_NOR_TRAD_NOR(0x1A) |\
FTIM1_NOR_TSEQRAD_NOR(0x13))
#define CONFIG_SYS_NOR_FTIM2 (FTIM2_NOR_TCS(0x4) | \
FTIM2_NOR_TCH(0x4) | \
FTIM2_NOR_TWPH(0x0E) | \
FTIM2_NOR_TWP(0x1c))
#define CONFIG_SYS_NOR_FTIM3 0x0
Please refer to https://community.nxp.com/docs/DOC-333350 for details.
Thanks,
Yiping
Hi yipingwang,
RCW is programmed at the beginning of flash, external memory (0xE8000000).
If RCW is hardcoded, stored in Inside processor. So, 0xE8000000 - 0xE801FFFF will free. So, I am planning to flash uImage from 0xE8000000 instead of 0xE8020000.
I configured u-image load address in T4240RDB.h file,
"setenv loadaddr 0xe8000000;"
Is there any other configuration to I need do for changing the uImage start address apart from the board configuration?
Thanks & Regards,
VinothS
You could define NOR flash memory map according to your own requirement.
Thanks,
Yiping
Thank you for your reply.
Regards,
VinothS
Hi Yiping,
Thank you for your reply. I will update soon.
Regards,
VinothS.