hello,
i use the S12ZVLA128 MCU development a product ,now i have a problem.
i set the internal-bus-clock 24MHZ, CAN bit-rate is 500Kbps. then i want use the Timer module(TIM16B6CV3),i need a 1ms interrupt ,because i want do someting in the TIM_interrupt_ISR (for example :switch I/O every 1ms, send a CAN message every 10ms) . i disable the precision-timer ,the prescaler maxvalue is bus-clock/128 ,so the Timer frequency is 24000000/128=187500,period is 5.3us ;this can't meet my requirements ,so,what should i do ? thank you very much!
haiyang
2019-0709
Hello,
You can refer to this example:
Example S12ZVL ADC0 triggered by TIM0 OC updates PWM duty cycle
The OC is 25ms in this case.
BR, Daniel
I meant that you need 1ms interrupt period, right? 1ms perfectly fits into 16bits timer running at 24MHz.
24M / (1/1ms) = 24000, which is much less than you have in 16bits timer, which has pow(2, 16)=65536 of timer ticks overflow period. So just go with this, you don't need prescaler.
Timer prescaler just increases jitter for input capture function and reduces resolution for output compare function. If you need 1ms interrupt then you perfectly fit timer period 24E6/(1/0.001) < 2^16.