Please refer to the following Community question:
Complete NOR firmware is provided at:
https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Flsdk.github.io%2Fcomponents.html
LSDK IMAGES
Thank you Ufedor:)
BR/Junfeng
There is no pre-built SD boot image for the LS2088ARDB.
Please use a debugger and restore NOR or QSPI firmware image available at:
LSDK IMAGES
On the LS2085ARDB/LS2088ARDB revisions D – F, switch SW9 bits 3:5 control which bank the SoC loads from when it powers up.
When SW9[3:5] = OFF-OFF-OFF - NOR Flash Bank 0 is selected. With this settings the NOR Flash bank 0 is started from address 0x580000000.