New Project can't find standard C libraries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

New Project can't find standard C libraries

Jump to solution
3,153 Views
luke_ludington
Contributor II

I created a new project in MCUxpresso and on build the include statements for the standard C libraries come back unresolved. Other includes in the include path work.

Labels (1)
1 Solution
2,507 Views
luke_ludington
Contributor II

I found a solution to this problem. I recreated the project as a C project and it now works (before it was configured as a C Static Library) Thanks for all your help ErichS

View solution in original post

10 Replies
2,508 Views
luke_ludington
Contributor II

I found a solution to this problem. I recreated the project as a C project and it now works (before it was configured as a C Static Library) Thanks for all your help ErichS

2,507 Views
BlackNight
NXP Employee
NXP Employee

Hi Luke,

thanks for reporting back on this! Glad to hear that it works now.

Erich

0 Kudos
Reply
2,507 Views
lpcxpresso_supp
NXP Employee
NXP Employee

What version of MCUXpresso IDE are you using? v11.0.0 provides a fix for this issue:

 MCUXpresso IDE v11.0.0 Now Available 

Fixed issue with IDE losing C library include paths. This did not prevent projects from building but meant that indexer-related functionality reliant on these paths would not work correctly (for instance trying to open a C library include file from the editor). This issue could also cause Newlib projects to sometimes appear to be using Redlib include files.
Note: Existing projects can be "fixed" using Tools->Fixup Parsers option on the Project Properties view's context sensitive menu

Regards,

MCUXpresso IDE Support

0 Kudos
Reply
2,507 Views
luke_ludington
Contributor II

Just downloaded v11 and set up my project and it still isn't working.

0 Kudos
Reply
2,506 Views
BlackNight
NXP Employee
NXP Employee

this is what helped for my projects:

1) right-click on the project and use Tools > Fixup Parsers

pastedImage_1.png

2) checking the Paths and Symbols for the project and removing any references to the IDE or previous IDE installation:

pastedImage_2.png

3) Checking that there is an 'MCU GCC Built-In Compiler parser' present pointing to the Include folders in the IDE:

pastedImage_3.png

4) Doing a Index rebuild on the project:

pastedImage_4.png

I hope this helps,

Erich

2,506 Views
luke_ludington
Contributor II

The MCU GCC Built-In Compiler parser doesn't show up how do I add it?

0 Kudos
Reply
2,506 Views
BlackNight
NXP Employee
NXP Employee

it should get added with the menu Tools > Fixup Parsers

can you retry?

0 Kudos
Reply
2,506 Views
luke_ludington
Contributor II

pastedImage_3.png

I can't seem to delete these references to the IDE, I tried your given process a few times. Thanks for all of your quick responses so far.

0 Kudos
Reply
2,506 Views
BlackNight
NXP Employee
NXP Employee

Strange.

This is what I had: I selected the item pointing to 10.3.1 and used the 'Delete' button.

pastedImage_1.png

This is not possible for you (you did not share the state of the button)? Or what do you get (error message?).

Erich

0 Kudos
Reply
2,506 Views
luke_ludington
Contributor II

Yeah the delete button is greyed out and the delete key does nothing

0 Kudos
Reply