Hi
I'm very confused ..
I started with imx6ullEVK generating a BSP and a simple application coming from CodeAurore repository.
https://source.codeaurora.org/external/imx/imx-manifest
imx-manifest - i.MX Release Manifest
And all is working ...
Now I saw the Freescale BSP community
GitHub - Freescale/fsl-community-bsp-platform: BSP platform manifest
and I tried to generate a BSP but without success.
But the questions is ...
Why two different methods to build images? And which one should I use?
Thanks
Fabio
Hello,
Please look at the following:
https://community.nxp.com/thread/323782
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank
I had already red that discussion but I was not sure about CodeAurora is equal to Yocto Community BSP ...
Is it real the same?
Thanks
Fabio
Hello,
The CodeAurora provides official NXP BSPs.
Look at Linux documentation: i.MX_Yocto_Project_User's_Guide.pdf,
i.MX_BSP_Porting_Guide.pdf.
https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS
Regards,
Yuri.
many thanks
Fabio