Freescale BSP community VS CodeAurora

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale BSP community VS CodeAurora

2,953 Views
fabio_poiatti
Contributor III

Hi

I'm very confused ..

I started with imx6ullEVK generating a BSP and a simple application coming from CodeAurore repository.

https://source.codeaurora.org/external/imx/imx-manifest

imx-manifest - i.MX Release Manifest 

And all is working ...

Now I saw the Freescale BSP community

GitHub - Freescale/fsl-community-bsp-platform: BSP platform manifest 

and I tried to generate a BSP but without success.

But the questions is ... 

Why two different methods to build images? And which one should I use?

Thanks

Fabio

0 Kudos
Reply
4 Replies

1,962 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Please look at the following:

https://community.nxp.com/thread/323782 


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,962 Views
fabio_poiatti
Contributor III

Thank

I had already red that discussion but I was not sure about CodeAurora is equal to Yocto Community BSP ...

Is it real the same?

Thanks

Fabio

0 Kudos
Reply

1,962 Views
Yuri
NXP Employee
NXP Employee

Hello,

   The CodeAurora  provides official NXP BSPs.

Look at Linux documentation: i.MX_Yocto_Project_User's_Guide.pdf,

i.MX_BSP_Porting_Guide.pdf.

https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS

 

Regards,

Yuri.

0 Kudos
Reply

1,962 Views
fabio_poiatti
Contributor III

many thanks

Fabio

0 Kudos
Reply