IEEE1588 on i.MX6Solox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEEE1588 on i.MX6Solox

Jump to solution
704 Views
linzhou
Contributor II

Hi bpe,

Our project uses the i.MX6SoloX processor. In the IEEE1588 application, I didn't find more references in the datasheet and reference manual.I have the following questions that need your support.:
1. I understand IEEE1588, there should be similar pins such as 1588_CLK_IN, 1588_PULSE_OUT, but I have not found similar pins in the i.MX6SoloX processor. The pins related to IEEE1588 are only ENETn_1588_EVENTn_IN and ENETn_1588_EVENTn_OUT. How to connect these pins correctly?
2. Do I need to add an external high precision reference clock source separately? Is it possible to pass the ENETn_1588_EVENTn_IN pin if needed?
3.Is the 1 PPS signal output directly through the ENETn_1588_EVENTn_OUT pin?

 

Thanks very much for your reply!

0 Kudos
Reply
1 Solution
636 Views
Yuri
NXP Employee
NXP Employee

Hello,

  please refer to the following: https://community.nxp.com/thread/486148 

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
1 Reply
637 Views
Yuri
NXP Employee
NXP Employee

Hello,

  please refer to the following: https://community.nxp.com/thread/486148 

Regards,

Yuri.

0 Kudos
Reply