ERR005723 PCIe: PCIe does not support L2 Power Down
Description:
When PCIe works as Root Complex, it can exit L2 mode only through reset. Since PCIe doesn't have a dedicated reset control bit, it cannot exit L2 mode.
Projected Impact:
PCIe does not support L2 Power Down
Workarounds:
The PCIe can be put in PDDQ mode to save on PCIe PHY power and wakeup only by the OOB (Out of Band) wakeup signal (since wakeup by a beacon from link partner is not supported) driven from the link partner (End Point). This signal could be used as a GPIO interrupt to exit this mode.
The limitation of this workaround is that the link partner cannot be put into L2.
Proposed Solution:
No fix scheduled
Linux BSP Status:
No software workaround available
* PCIe controller doesn’t have the reset mechanism that can be used when re-insmod the PCIe driver without power down/up PCIe module.
* During the PCie driver rmmod/insmod operations, the PCIe CLKs would be turned off/on. IC can’t guarantee that the PCIe PHY can work well and re-establish the PCIe link properly.
One SIMPLE SW workaround for this errata
imx: pcie: toggle bit18 of grp1 fix pcie can't exit L2 issue.
Set bit18 of gpr1 before enter into supend, and clean it
after resume, can fix the following errata.
Errata ERR005723_PCIe PCIe does not support L2 Power Down.
About the details, please refer to the attached patch.
"0001-imx-pcie-toggle-bit18-of-grp1-fix-pcie-can-t-exit-L2.patch"
* UART
* ENET
* PCIe
one i.MX6Q SD boards, and one INTEL pciex1 1000M CT network card.
Kernel is based on imx_3.0.35_4.0 release, uboot , is based on imx_v2009.08
# unload ep's driver --> suspend/resume --> reload ep's driver.
Please make sure that the command line contains “no_console_suspend”
The command used to enable the console input wake up after login the consol:
echo enabled > /sys/devices/platform/imx-uart.0/tty/ttymxc0/power/wakeup
-------------------------------log--------------------------------------------
PM: Syncing filesystems ... done. start suspend
Freezing user space processes ... (elapsed 0.01 seconds) done.
Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.
add wake up source irq 101
add wake up source irq 99
add wake up source irq 103
add wake up source irq 51
add wake up source irq 58
PM: suspend of devices complete after 15.482 msecs
PM: late suspend of devices complete after 0.823 msecs
Disabling non-boot CPUs ...
CPU1: shutdown
CPU2: shutdown
CPU3: shutdown
IMX PCIe imx_pcie_pltfm_suspend entering.
IMX PCIe imx_pcie_pltfm_suspend exit. suspended
U-Boot 2009.08-00679-g6ec6783 (May 20 2013 - 14:50:20) resume
CPU: Freescale i.MX6 family TO1.2 at 792 MHz
src 0x92eac8
resume 0x92eac8
jump to resume
IMX PCIe imx_pcie_pltfm_resume entering.
IMX PCIe imx_pcie_pltfm_resume pcie start re-link.
IMX PCIe port imx_pcie_pltfm_resume: re-link up.
Enabling non-boot CPUs ...
CPU1: Booted secondary processor
Calibrating delay loop (skipped) already calibrated this CPU
CPU1 is up
CPU2: Booted secondary processor
Calibrating delay loop (skipped) already calibrated this CPU
CPU2 is up
CPU3: Booted secondary processor
Calibrating delay loop (skipped) already calibrated this CPU
CPU3 is up
PM: early resume of devices complete after 0.974 msecs
remove wake up source irq 58
imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
remove wake up source irq 51
remove wake up source irq 103
remove wake up source irq 101
remove wake up source irq 99
PM: resume of devices complete after 54.174 msecs
Restarting tasks ... done.
PHY: 1:01 - Link is Up - 100/Full resume is ok, reload ep’s driver
num is 61
e1000e: Intel(R) PRO/1000 Network Driver - 1.3.10-k2
e1000e: Copyright(c) 1999 - 2011 Intel Corporation.
e1000e 0000:01:00.0: Disabling ASPM L0s
e1000e 0000:01:00.0: (unregistered net_device): Failed to initialize MSI-X interrupts. Falling back to MSI interrupts.
e1000e 0000:01:00.0: (unregistered net_device): Failed to initialize MSI interrupts. Falling back to legacy interrupts.
e1000e 0000:01:00.0: eth1: (PCI Express:2.5GT/s:Width x1) 00:1b:21:3a:18:8b
e1000e 0000:01:00.0: eth1: Intel(R) PRO/1000 Network Connection
e1000e 0000:01:00.0: eth1: MAC: 3, PHY: 8, PBA No: E42641-005
e1000e: eth1 NIC Link is Up 1000 Mbps Full Duplex, Flow Control: Rx/Tx
PING 192.168.0.1 (192.168.0.1): 56 data bytes
64 bytes from 192.168.0.1: seq=0 ttl=64 time=3.126 ms
64 bytes from 192.168.0.1: seq=1 ttl=64 time=0.244 ms
64 bytes from 192.168.0.1: seq=2 ttl=64 time=0.232 ms
64 bytes from 192.168.0.1: seq=3 ttl=64 time=0.206 ms
64 bytes from 192.168.0.1: seq=4 ttl=64 time=0.222 ms
64 bytes from 192.168.0.1: seq=5 ttl=64 time=0.207 ms
64 bytes from 192.168.0.1: seq=6 ttl=64 time=0.250 ms
64 bytes from 192.168.0.1: seq=7 ttl=64 time=0.209 ms
64 bytes from 192.168.0.1: seq=8 ttl=64 time=0.154 ms
64 bytes from 192.168.0.1: seq=9 ttl=64 time=0.211 ms
--- 192.168.0.1 ping statistics ---
10 packets transmitted, 10 packets received, 0% packet loss
round-trip min/avg/max = 0.154/0.506/3.126 ms
PM: Syncing filesystems ... done. ep’s functions are ok, re-do the suspend/resume tests
Freezing user space processes ... (elapsed 0.01 seconds) done.
-------------------------------end--------------------------------------------
Original Attachment has been moved to: 0001-imx-pcie-toggle-bit18-of-grp1-fix-pcie-can-t-exit-L2.patch.zip
Original Attachment has been moved to: uboot_patch_image.zip
Original Attachment has been moved to: kernel_patch_image.zip