This porting guide is for FRDM-K82F, and it can also be used for any other platform supported by KSDK 2.2.
The released NXPNCI-KDS_Example_KSDK2.2 is based on FRDM-K64F, so before porting, we need to configure and download KSDK 2.2 for FRDM-K82F.
Please make sure you have selected Kinetis Design Studio before downloading.
After downloading, extract the package to some folder like below:
and change PROJECT_KSDK_PATH to this folder:
Change project settings as below:
Remove all files in the folder of drivers, and import new source files as below:
and similar procedure for "startup" folder and "utilities" folder:
Replace the source files in board folder with the files from some ksdk demo like hello_world:
FRDM-K82F uses PTC3 for NCI_IRQ pin, PTC9 for NCI_VEN pin, and PTA1 and PTA2(I2C3) as the I2C interface. so add definition in board.c and modify BOARD_InitPins() as below:
Change linker settings:
-Build
-Debug settings
-Test Result: