AUT-N1783 Hands-On Workshop Secure CAN Networks

File uploaded by Lisa Hughes Employee on May 25, 2016Last modified by Renee Fortenberry on Dec 18, 2018
Version 3Show Document
  • View in full screen mode

The modern car has already gone beyond a simple mode of transportation to a platform for connectivity. The challenges of balancing performance and cost have the new requirement to meet security as the car becomes connected to the rest of the world. This class will review the security implications for CAN communications. The class will walk through a hands-on connecting a CAN network of two MPC5748G devices via secure CAN communications. Leveraging the SHE firmware on the MPC5748G HSM. CAN messages with be signed before transmission and authenticated on the receiving end using CMAC and AES-128.

Outcomes