U-boot FW Printenv FW Env File

Document created by jesseg Employee on Jul 30, 2012Last modified by Jodi Paul on May 16, 2013
Version 5Show Document
  • View in full screen mode


# Configuration file for fw_(printenv/saveenv) utility.

# Up to two entries are valid, in this case the redundant

# environment sector is assumed present.

# Notice, that the "Number of sectors" is ignored on NOR.


# MTD device name Device offset Env. size Flash sector size Number of sectors

#/dev/mtd1 0x0000 0x4000 0x4000

#/dev/mtd2 0x0000 0x4000 0x4000

# NAND example

/dev/mtd0 0x80000 0x40000 0x20000 2