APF-SNT-T1359

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

APF-SNT-T1359

APF-SNT-T1359

The QorIQ T1040 and T1042 communication processors support four integrated 64-bit e5500 Power Architecture® processor cores with high-performance data path acceleration architecture (DPAA) and network peripheral interfaces required for networking and telecommunications. This session will provide an in-depth look at the new features being introduced in the T1040 family such as the Single Source Clock, L2 Switch, sSDXC, QSGMII and DDR4. The session will also cover power-saving schemes of T1040.

Presented by duchen-b44125

Presented at DwF Digital Networking - Nanjing - 21 May 2015

Session ID: APF-SNT-T1359

Attachments
No ratings
Version history
Last update:
‎05-27-2015 04:35 PM
Updated by: