Hi
I cannot get any way to map a variable to a specific section to work.
Memory section is created by processor expert, here it is called mysection
From processorexpert.lcf
MEMORY { interrupts (RX) : ORIGIN = 0x1FFF0000, LENGTH = 0x000001E0 code (RX) : ORIGIN = 0x1FFF01E0, LENGTH = 0x00015220 data14000000 (RW) : ORIGIN = 0x14000000, LENGTH = 0x00001000 data (RW) : ORIGIN = 0x20005400, LENGTH = 0x00006C00 mysection (RW) : ORIGIN = 0x2000C000, LENGTH = 0x00004000 cfmprotrom (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010}
Here are some traces on what I have tried to map a variable to "mysection"
#pragma define_section MYSECTION ".bss" far_absolute RW//#pragma section MYSECTION begin//uint16_t adcIn[8192] __attribute__ ((align (8));uint16_t adcIn[8192] __attribute__ ((section ("MYSECTION")));//__declspec(MYSECTION) uint16_t adcIn[8192];//uint16_t adcIn[8192];//#pragma section MYSECTION end
The compilation/linking is OK, but the variable "adcIn" maps to section "data" no matter what.
Any ideas?
Solved! Go to Solution.
#pragma define_section MYSECTION ".mysection" abs32 RW__declspec(MYSECTION) uint16_t adcIn[8*2*512];/* lcf file .mysection : { __START_MYSECTION = .; * (.mysection) __END_MYSECTION = .; . = ALIGN(0x4); } > mysection*/
The above is working, but ProcessorExpert must be configured to not generate linker file due to the manually added code in lcf file.
By the way, the following code makes CW10 arm compiler to crash:
#pragma define_section MYSECTION ".sec1" ".sec2" ".sec3" ".sec4" far_absolute RW
#pragma define_section MYSECTION ".mysection" abs32 RW__declspec(MYSECTION) uint16_t adcIn[8*2*512];/* lcf file .mysection : { __START_MYSECTION = .; * (.mysection) __END_MYSECTION = .; . = ALIGN(0x4); } > mysection*/
The above is working, but ProcessorExpert must be configured to not generate linker file due to the manually added code in lcf file.