Hi,
I see a relation between frequency and resolution in the PWM module. Is there any equation for this with a S08SH? Any way to know how many time I need to reach a desired resolution?
I would like to generate a 200KHz PWM with more than 8 bits resolution, is it possible directly with a S08SH?
Thanks.
Solved! Go to Solution.
Hello,
To achieve 8-bit PWM resolution at 200kHz frequency would require a TPM clock frequency of 256 * 200 kHz, or 51.2 MHz. This is clearly not feasible with 8-bit MCU devices.
Regards,
Mac
Hello,
To achieve 8-bit PWM resolution at 200kHz frequency would require a TPM clock frequency of 256 * 200 kHz, or 51.2 MHz. This is clearly not feasible with 8-bit MCU devices.
Regards,
Mac
Ok, thanks for the aclaration.