Hello:
I downloaded a free trial of Codewarrior for HC12 and I can generate .lst files with no problerm.
Tha problem is with CodeWarrior 5.9.0 build 3510.
It has no option to generate the .lst file in all the menus. In fact a lot of menus are different than HC12's Codewarrior.
Basically I want to know the equivalent C-Assembly generated code just like a plain .lst file.
Anyone knows how to do that on Codewarrior for MPC55xx?
Thanks
Solved! Go to Solution.
Hi robertin75,
CodeWarrior for MPC55xx can generate disassembly listing for a c file as well.
In the IDE project manager select a file, right click and select "Disassemble". If you wish to see mixed C/asm listing you have to enable "Show Source Code" option in the project settings (ALT + F7 -> "Code Generation" -> "EPPC Disassembler" -> "Show Source Code" check box)
Stanish
Hi robertin75,
CodeWarrior for MPC55xx can generate disassembly listing for a c file as well.
In the IDE project manager select a file, right click and select "Disassemble". If you wish to see mixed C/asm listing you have to enable "Show Source Code" option in the project settings (ALT + F7 -> "Code Generation" -> "EPPC Disassembler" -> "Show Source Code" check box)
Stanish
Hey thanks a lot Stanish !!
Just was I was looking for.