Hi ,
I am using coldfire IDE 5.7.0 version. While compiling a workspace I am getting error "Cannot open stdio.h" .
It looks to me , coldfire project , not getting stdio.h file path."C:\Program Files\Freescale\CodeWarrior for ColdFire V6.4\E68K_Support\" . Could you please let me know how I can include this path.I am using MCF 5485 based hardware.For your reference, here I am attching the error log as a jpg file
Thanks,
Sethu
Hello
If you create your project using a stationery or the wizard, Access Paths settings should be appropriate.
If you need to add the path to your system include files, proceed a follows:
- Open the Target settings dialog (Press ALT+F7)
- Go to Target > Access Paths
- Check System Paths radio button
- Then click Add ... The Browse for Folder dialog is opened.
- Make sure Compiler Relative is specified as Path Type then browse for the include file directory.
- Click on OK to close the Browse for Folder dialog.
- Click on OK to close the Target Settings dialog.
Crasycat
I am able to compile now. But I am getting following link error.
Linker command file not found
Making default command file (see link map)
Link Error : Undefined : "_start"
Could you please guide me how to correct this error.
Thanks,
Sethu
Hello
You seem to have a big problem with your project.
I would recommend you to create a new project using the wizard and then add your own source files to the new project.
This will probably save you a lot of time.
CrasyCat