I get this error
ERROR L1100: Segments ROM (0x8000) and FLASH_TO_RAM (0xE000) overlap
When compiling for HC08
this is a piece of the prm file
/* This is a linker parameter file for the GT32 */NAMES END /* CodeWarrior will pass all the needed files to the linker by command line. But here you may add your own files too. */SEGMENTS /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */ ROM = READ_ONLY 0x8000 TO 0xFFAF; Z_RAM = READ_WRITE 0x0080 TO 0x00FF; RAM = READ_WRITE 0x0100 TO 0x087F; ROM1 = READ_ONLY 0xFFC0 TO 0xFFCB; FLASH_TO_RAM = READ_ONLY 0xE000 TO 0xE00F RELOCATE_TO 0x0200; ENDPLACEMENT /* Here all predefined and user segments are placed into the SEGMENTS defined above. */ DEFAULT_RAM INTO RAM; DEFAULT_ROM, ROM_VAR, STRINGS INTO ROM; /* ROM1 In case you want to use ROM1 as well, be sure the option -OnB=b is passed to the compiler. */ _DATA_ZEROPAGE, MY_ZEROPAGE INTO Z_RAM; FLASH_ROUTINE INTO FLASH_TO_RAM;ENDSTACKSIZE 0x250 ... ...
It worrks great in Codewarrior 5.9, but don't compile and gives ERROR L1100 in Codewarrior 10.0
Any Ideas of how to solve this?
Thanks in advance!
Don't use the same memory range twice....
I guess for CW classic (5.9 is the ide version, latest is version 6.3) the error is just suppressed but basically still there.
I would suggest to move FLASH_TO_RAM to 0xFFA0..0xFFAF and change the ROM segment to end at 0xFF9F.
Depending on how the (C or assembly) source code is written, it might contain the 0xE000 address too, has to be adapted as well.
Daniel