I tried copying the MQX.DLL C:\Freescale\CW MCU v10.1\MCU\bin\plugins\Debugger\rtos directory, but it did not work.
I believe I am running the full pro license.
Brynn
Solved! Go to Solution.
Hi,
unfortunatelly MQX 3.6.2 TAD does not support with CodeWarrior 10.1 Beta. The TAD for CW 10.1 is planned for the next MQX version.
Regards,
PetrL
Hi,
unfortunatelly MQX 3.6.2 TAD does not support with CodeWarrior 10.1 Beta. The TAD for CW 10.1 is planned for the next MQX version.
Regards,
PetrL
PetrL, I also have the released 10.1 IDE installed. Trying to manually add the MQX extensions from MQX 3.6.2 does not work. When will we see MQX 3.7.0 so I can start using the 10.1 IDE?
Hi Kelly,
End of March is our ETA.
Regards,
David
David,
Until MQX 3.7.0 is released, what is the recommended IDE for Coldfire V2 MQX?
I'd prefer to use CW 10.0 eClipse since it will probably be the platform moving forward, and seems to have a more expanded new project wizard, but I have not found it available for download anywhere.
Thanks and Kind regards,
Erik Strack
Okay, Now the CW 10.1 release is out, not just the Beta anymore. I see the TAD is still not there Are you saying that I need to wait for a MQX 3.6.3 or a 3.7 before we get the Task Aware Debugging feature back? When might that be?
Also, the new project wizard that was aware of MQX seems to be gone. Should I be concerned that Freescale might drop MQX?
Brynn