Hi,
I try to decrease current consumed by MCU (MCF52255). I define two functions for that. First function turns MCU in low power Stop mode (deepest mode). Here is code for this action:
The second function turns MCU in low power Wait mode. In this mode, I want CPU answers to interrupts. Here is code for this action:
MCF_PMM_LPCR = MCF_PMM_LPCR_LPMD_WAIT; // Select wait mode
MCF_PMM_LPICR = 0
| MCF_PMM_LPICR_XLPM_IPL(0) // Any level can wake up MCU
| MCF_PMM_LPICR_ENBSTOP; // Activate low power mode
asm( stop #0x2000);
If I use wait or stop function, when MCU is idle and FEC is not used (MCU does not wait for a FEC interrupt), that works well. When FEC is not used, external PHY is in Power Down mode.
There is a problem when I want use wait function when MCU is idle and FEC is used: I don't know why, but Backup Watchdog Timer (BWT) resets MCU in this case (RSR register has 0x80 after MCU reset).
Do you have hints for me?
Thanks,
Steve
Other information
BWT counter is reset in RTC interrupt. RTC interrupt increment my SystemTick and it has frequency of 1000 Hz.
FEC interrupt seems cause problem to RTC interrupt... That's strange.
Steve