Fractional arithemtic on DSP56F803

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fractional arithemtic on DSP56F803

1,616 Views
weberti
Contributor I

Hi everybody,

 

I had to implement a controller (for DSP56F803) which was designed with floating point numbers, but it took too much time to execute. So I started to look and I've found the Fractional arithmetic as a possible solution, but something really goes wrong with the basics.

Can somebody help me if I am on the right track?

I am using Metrowerks CodeWarrior 7.0 to compile and I've found the intrinsics_56800E.h, which is referenced at many sources, but it seems it doesn't work with my assembler. It complains about "unknown assembler instruction mnemonic" for example in case of ".optimize_iasm". 

Is this header can be used with my processor at all!? I guess that is the first thing that I've need to find out. Does anybody have an idea?

 

If I am on the wrong path, then is there anybody who can give some hint which direction to start?

 

Thanks in advance,

 

// Tibor

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

506 Views
weberti
Contributor I
So it seems. It won't work. The .h is specificly for 56800E (as the name states) and the things I am looking for are not supported on 56F803.
0 Kudos
Reply

506 Views
trytohelp
NXP Employee
NXP Employee

Hi,

 

Intrinsic functions ares supported be DSC tool.

Please have a look to the Targeting_56800.pdf manual.

there is a chapter for that:

Inline Assembly Language and Intrinsic Functions

List of Intrinsic Functions: Definitions and Examples

Hope this will help you.

Regards

Pascal Irrle 

 

 

0 Kudos
Reply