Flashing MPC8536DS with CW 8.8.2 and USB TAP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing MPC8536DS with CW 8.8.2 and USB TAP

1,617 Views
StefanBohne
Contributor I

I need to upload u-boot into the flash of a MPC8536DS board, but CodeWarrior 8.8.2 does not even know the 8536 processor. I've been using the configuration files from http://forums.freescale.com/freescale/board/message?board.id=CWCFCOMM&thread.id=2693, but it doesn't work.

 

Does anybody know where how to tell CW about the 8536 or have another idea? Any help would be greatly appreciated.

Labels (1)
0 Kudos
Reply
3 Replies

499 Views
StefanBohne
Contributor I

I've checked it again, and it is version 1.0.

 

The problem is, that I can't select the proper processor in Flash Programmer. The 8536 is not listed under Target Processor.

0 Kudos
Reply

499 Views
ronco
NXP Employee
NXP Employee

For the Flash Programmer the exact processor selection is often not necessary.  Load in the MPC8536___.xml file you want then set the Processor Family to '85xx' and the Target Processor to '8533'.  That should work.

 

-Ron

0 Kudos
Reply

499 Views
J2MEJediMaster
Specialist I

Per the forum thread that you referenced, what rev of the board do you have? Those patches will not work with a rev 1.1 board.

 

---Tom

 

Message Edited by J2MEJediMaster on 2009-06-19 11:19 AM
0 Kudos
Reply