The command-line assembler supports an option '-list' to generate an assembly listing file. This is generated in the directory where the source-file is located.
However, this conflicts with the basic possibility to generate two or more variants from the same
source tree (say, release and debug). Is it possible to indicate a separate directory for producing such
listing files (like is possible for object files, indicating a pathname to the '-o' option)?
At the moment, if i start two different builds (debug and release, using the same source tree) simultaneously, one may break since it cannot write the *.list file while the other build is also generating this list file.
Also, I currently cannot generate the project if the source tree is read-only, e.g. from a CD-ROM backup...
TIA,
Johan
Hello
I would suggest you to submit a Change Request for that through our on-line support web site.
I would recommend you to submit a service request for that.
Click here to submit a service request.
CrasyCat