current, I use cw for coldfire V7.1, But it seem to something wrong when I use it with tblcf BDM. I doubt the v7.1 CW is not enough steady. so I want to try v6.4 or v6.3, but where I can get them?
thanks!
Before attemtping to fall back a version, do you have the latest patch installed for CW for ColdFire 7.1? The 7.1.1 patch can be found here. The release notes mention several fixs for OSBDM support, and they might apply to your interface as well.
---Tom
When you build the program, are you using the INTERNAL_FLASH target? The other two target types (INTERNAL_RAM and CONSOLE_INTERNAL_RAM) have the program reside in RAM memory and not flash, so nothing will happen to flash memory. Have you tried just letting the program execute and see what happens?
---Tom
Hi. I try to build project with INTERNAL_FLASH target. and then program into flash, but error occured.
I also try to build it with INTERNAL_RAM and CONSOLE_INTERNAL_RAM target and then press F5 to execute. the mcu seems to be halted, never execute instruction.