what will cause RCM_SRS_SW_MASK (software) reset?
Hi 78621251@qq.com,
This is a software reset.
https://community.nxp.com/message/1115254
Regards,
Daniel
Which registers can be cleared manually for non power-on reset so that they are the same as power-on reset status
There is no list of registers that are cleared on POR only.
Each registers has its own specification.
For example:
Regards,
Daniel
Hi 78621251@qq.com,
Some registers are reset only on power-on reset.
Could you read the RCM_SRS during startup to find the source of the reset?
Thanks,
BR, Daniel
RCM_SRS_PIN_MASK this reason again and again
Hi 78621251@qq.com,
If you see RCR_PIN = 1, that means that another device connected to the reset_b pin is the cause of the reset, not the MCU itself.
Regards,
Daniel