PN7462 temperature issues over 50°C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 temperature issues over 50°C

751 Views
jeanlucchaillat
Contributor II

Hi everybody,

I developed a custom card reader for contact and contactless smart card, this card reader is expected to run in an outdoor environment and with a temperature up to 70°C

I have issues when the ambient temperature goes over 50°C with contact cards.

The issues are :

  • ATR is corrupted or
  • During APDU exchanges, frames are corrupted.

 

The NXP data sheet says the PN7462 should work up to 85°C

The firmware of the reader comes from the NXP example PN7462AU_ex_phExCcid where the 2 temperature sensors of the PN7462 are disabled.

 

Does anyone met similar issues? Any idea ?

 

Regards,

 

Jean-Luc Chaillat

Tags (1)
0 Kudos
1 Reply

704 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

can you check that all the other components are properly solder and are working properly? Please check that the external crystal is working properly.

Have a good day

0 Kudos