MRF6V3090N design for 1025-1150 MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRF6V3090N design for 1025-1150 MHz

561 Views
raveendrareddy
Contributor II

Hi Team,

would you please share any design which is available for the frequency band of 1025 - 1150 MHz by using device MRF6V3090N? I would like to use this device for the frequency band 1025 - 1150 MHz

Labels (1)
  • RF

Tags (1)
0 Kudos
Reply
1 Reply

527 Views
LPP
NXP Employee
NXP Employee


NXP offers MRF6V3090N Reference Circuit, 90W Pulse @ 915-1215 MHz

You can request documentation pack including layout and performance report for this board using our service "RF Circuit Collection"
https://www.nxp.com/design/development-boards/rf-circuit-collection:RF-CIRCUIT-COLLECTION

Also, you can order board from our distributors.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply