Hi,
I would like to add Mifare support for my iOS app and ran into some problems. Concretely I would like to read the Mifare-Card's UID.
As far as I got, I need to pass some "Application Identifiers" (AID?) into the info.plist to get the tagReaderSession to callback. What is / are the AIDs for Mifare classic 1K, Mifare Classic 4K, Mifare Plus EV1, Mifare Ultralight EV1, Mifare Desfire EV1 and Mifare Plus EV1?
I would be very happy about any kind of help!
Hi Heini Müller,
Hope you are doing great, as you may know IOS supports the NDEF interaction,
Unleash the full potential of NFC with iOS 13 and NXP | NXP
I am not sure if you mean the DF names and the file IDs, as you may know when you have a type 4 tag there is a certain file structure to comply with the 7816-4 please check for example our NTAG 424 which has preloaded this type of structure for more information please check the ISO 7816-4 spec
BR
Jonathan