Recently, the end customer has proposed the requirement of electrical transient conduction immunity along the signal line / control line.
The question:Can the TJA1052iT meet the Standard: Test in accordance with GB / T 21437.3-2012 (ISO 7637-3)?
Meet Class III requirements: The device or system can perform all its pre-designed functions during and after the harassment.
Schematic diagram:
可以满足的这个测试规则。
稍等我给你一个EMC测试的报告供参考通过邮件的方式
Hi G.w.Sun
I have received the file, thank you for your support!
Best regards
Field Application Enginner – Mingsong Yang