Hello,
I'm developing one product using UJA1132HW3V3 and S32K148. I'm trying to configure the HVIOs on UJA1132HW3V3 as wake up inputs and trying to read the status of the wake up input.
However, I got full zeros when using SBC_Transfer function in SDK to access the "Bank 0 wake-up status register" and "Bank 1 wake-up status register".
Meanwhile, I also could not read out the HVIOn(1-4, and 5-8) control registers using the SBC_Transfer function.
Can you support me on this topic? Thanks!
My SDK version is: S32SDK_S32K1xx_RTM_3.0.0
Hello 13681887479@163.com,
Hard to say, it could be a HW issue.
Do you monitor the SPI bus with an oscilloscope?
Have you tried the sbc_uja113x_s32k148 SDK example?
Does it work?
Thanks,
BR, Daniel