imx8: QT app failing on imx8mq-evk, wayland-egl plugin loading failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8: QT app failing on imx8mq-evk, wayland-egl plugin loading failed

2,083 Views
vsuneja63
Contributor III

I am running camera qt app on imx8mq-evk target. Facing below logs while clicking on app:

Mar 06 09:54:27 imx8mqevk afbd-camera@0.1[4392]: Failed to create wl_display (Permission denied)
Mar 06 09:54:27 imx8mqevk afbd-camera@0.1[4392]: Using Wayland-EGL
Mar 06 09:54:27 imx8mqevk afbd-camera@0.1[4392]: EGL: Warning: No default display support on wayland
Mar 06 09:54:27 imx8mqevk audit[4393]: ANOM_ABEND auid=4294967295 uid=1001 gid=1001 ses=4294967295 subj=User::App::camera pid=4393 comm="camera" exe="/var/local/lib/afm/applications/camera/0.1/bin/camera" sig=6 res=1
Mar 06 09:54:27 imx8mqevk afbd-camera@0.1[4392]: EGL not available
Mar 06 09:54:27 imx8mqevk afbd-camera@0.1[4392]: qt.qpa.plugin: Could not load the Qt platform plugin "wayland-egl" in "" even though it was found.
Mar 06 09:54:27 imx8mqevk afbd-camera@0.1[4392]: This application failed to start because no Qt platform plugin could be initialized. Reinstalling the application may fix this problem.
Mar 06 09:54:27 imx8mqevk afbd-camera@0.1[4392]: Available platform plugins are: minimal, offscreen, vnc, wayland-egl, wayland.

I tried reinstalling but same issue, am i missing any dependency package?

0 Kudos
Reply
3 Replies

1,942 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Vipul,

Which BSP are you using? Since EGL works as usual in the L5.4.3.

Regards

0 Kudos
Reply

1,942 Views
vsuneja63
Contributor III

Hi,

Thanks!

Waiting for your response. I am stuck with this issue, any update from your side will be a great help. Would like to hear from you on this.

Thanks & Regards,

Vipul Kumar

0 Kudos
Reply

1,942 Views
vsuneja63
Contributor III

Hi,

Thanks!

I am using linux-imx 4.19.35 . wayland-egl will work in this?

Thanks & Regards,

Vipul Kumar

0 Kudos
Reply