Hello,
Our platform based on I.MX6ull (Variscite DART 6ULL) with enabled 1 Ethernet port (of 2).
We would like to certificate our product, but we have got an EMC Ethernet issue.
During EMC tests we have observed 50MHz peak and its harmonics.
The disruption disappear when Ethernet went down (ifconfig eth0 down).
Is it possible to enable spread clock to Ethernet?
Best regards,
Kamil Zorychta
Hi Kamil
>Is it possible to enable spread clock to Ethernet?
sorry not possible as only PLL2 has spread spectrum, ENET
PLL6 has not such functionality, this is described in Chapter 18
Clock Controller Module (CCM)
i.MX 6ULL Applications Processor Reference Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for answer.
So we will focus on pin configuration to smooth signals edges. It may help.
Best regards,
Kamil