iMX7s USB suspend (peripheral mode)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7s USB suspend (peripheral mode)

1,250 Views
lucas_lin
Contributor I

Hi,

I set USB OTG to peripheral mode and to run some USB test.

About the suspend mode test.

When the host enter S3, the device (iMX7s) shall enter suspend mode too.

But my device still stay in run mode.


My question is if usb driver received suspend signal from host, can it make whole system enter suspend mode (suspend to ram) or just itself will enter suspend mode?

Thank you for your help.

Labels (2)
0 Kudos
Reply
3 Replies

1,170 Views
lucas_lin
Contributor I

Hi Bio,

Did you mean that when usb got suspend signal from host and enter suspend state, it will bring whole system enter suspend mode?
If yes, which configurations I need to set?
Because my EV-Board is always stay in run mode even the host already enter to S3.

Thank you.

0 Kudos
Reply

1,170 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Sorry No, If you don´t tell the board to enter suspend mode it won´t enter.

0 Kudos
Reply

1,170 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Lucas,

Yes, It will enter to suspend mode.

Regards

0 Kudos
Reply