I am using the MCIMX6Y2DVM microcontroller in my testing board, I am programming this controller manually using MFGtool2.exe. I want to automate the programming for my project. I am using LabVIEW an industrial automation tool where I am using a batch file that consists of command-line utility code which I took from the .vbs file in the MFGtool package folder. I have commands to program the board but the command prompt is not exiting after the completion of programming and the result if not appearing in a new instead it is just updating the number of successes and failures. the following in the command line I use in the batch file to programmer the controller.
cd "C:\Mfg_tool_and_binary_eol\mfgtools"
MfgTool2.exe -noui -c "linux" -l "eMMC" -p 1 -s "board=sabresd" -s "mmc=1" -s "6uluboot=14x14evk" -s "6uldtb=14x14-evk"
I want the command to exit the command prompt after the completion of the programming. And I also want a command to display the result in new line.khumphriMandardhavalRHinnenjimtrudeauMartinvladcenteamarc.paquetteRChapmanAlbani.MX Processors NXP Training Content
mx6 ullmcimx6ull#MFGtool2.exe
Hi igor,
firstly, Thanks for your response. I don't know to use this uuu tool, I could not find any executable file or .vbs file in the link you mentioned. can you please explain about the tool. igorpadykov Thank You
Hi M Harishankaran
please scroll down on below link, there one can find examples
GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools
pdf document can be found on
Releases · NXPmicro/mfgtools · GitHub
Best regards
igor
Hi M Harishankaran
mfg tool is not more supported, suggested to migrate to uuu tool
GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------