Hi All,
I am new to linux. I took the iso image for Lite5200b target and using ltib utility built the image for the target.But when I port the image to target I get the following output
=> tftpboot 0x200000 uImage
Using FEC ETHERNET device
TFTP from server 10.246.75.165; our IP address is 10.246.75.13
Filename 'uImage'.
Load address: 0x200000
Loading: #################################################################
#################################################################
#################################################################
################################################################
done
Bytes transferred = 1321215 (1428ff hex)
=> bootm
## Booting image at 00200000 ...
Image Name: Linux-2.6.16.11-rt18
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 1321151 Bytes = 1.3 MB
Load Address: 00000000
Entry Point: 00000000
Uncompressing Kernel Image ... OK
id mach(): done
MMU:enter
MMU:hw init
MMU:mapin
MMU:setio
MMU:exit
setup_arch: enter
setup_arch: bootmem
arch: exit
and after this the board resets.
Can you please let me know why this problem exists?
Thanks,
Srinivas
Check your kernel command line and make sure that you have set to console= correctly. For detailed instructions see the BSP User Manual on the bsp iso. The easiest way to access all of the bsp docs is via the START_HERE.html that is also on the bsp iso.
- Coray