i.MX7 USB_OTG2_VBUS voltage supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 USB_OTG2_VBUS voltage supply

Jump to solution
904 Views
m_c
Senior Contributor I

Is USB_OTG2_VBUS 5v still need to supply if i.MX7 USB2 only used in host mode and USB device 5v is supply externally?

pastedImage_1.png

Labels (1)
0 Kudos
1 Solution
824 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

>Is USB_OTG2_VBUS 5v still need to supply if i.MX7 USB2 only used in

>host mode and USB device 5v is supply externally?

no, it is not needed.

Best regards
igor
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
825 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

>Is USB_OTG2_VBUS 5v still need to supply if i.MX7 USB2 only used in

>host mode and USB device 5v is supply externally?

no, it is not needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos